最近在做关于CC3100的毕设,基于mbed平台,不知道大家了解么,其中提供了CC3000驱动在mbed平台下的移植,所以想问一下CC3000和CC3100的驱动是通用的么?想验证一下我的方案是否可行
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
嗯嗯,谢谢,是需要修改的,我还可以问一个问题么?CC3100做AP最多可以连接几个Wi-Fi子设备?我整套系统用的都是CC3100,智能网关中的CC3100做AP,需要和3个传感器模块上的CC3100相连做通信,CC3100能够满足么?刚在TI论坛看到一个帖子,说做实验发现CC3100做AP只能连接一个子Wi-Fi设备。
CC3100做AP可以连接1个Station。
同时更新一下WiFi CC3100/ CC3200的升级芯片CC3120/CC3220的基本信息:
The CC3220 family offers three pin-to-pin compatible variations:
CC3220SF芯片内置了 1MB的Flash,客户的代码直接在Flash中运行,256k的RAM完全开放给客户使用,同时增加了Security的支持
CC3220S芯片使用256k的RAM同时运行代码和RAM,也就是代码+程序使用的RAM在256k范围之内,增加了Security的支持
CC3220R芯片内置256k的RAM,
最新的CC3220升级芯片在AP模式下可以支持最大4个Station的连接,同时增加了IPV6的支持,增强了wifi RF的设计,大幅度提升了SmartConfig的配置成功率,详细了新特性的增加请参考CC3220的芯片手册和设计指南。
现在CC3100/3200做AP只能连接一个STATION,但是我毕设又需要采集三个子节点的数据,请问我现在该怎样实现这一功能呢?是不是只能换WiFi芯片了?用轮询的方式能实现么