This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] WPA3安全

Other Parts Discussed in Thread: WILINK8-WIFI-NLCP

Q1)什么是WPA3

A1)WPA3是下一代Wi-Fi安全标准,代表Wi-Fi保护访问,“ 3”是最新版本,WPA3是Wi-Fi身份验证标准WPA2技术的的后续版本

 

Q2)WPA3与WPA2有何不同?

A2)WPA3建立在WPA2广泛成功和采用的基础上,WPA3添加了新功能并删除了过时的旧协议。例如,WPA3用更安全的协议SAE(Simultaneous Authentication of Equals)代替了WPA2预共享密钥机制。此外,WPA3要求使用受保护的管理框架(PMF),这有助于增强Wi-Fi安全性。WPA3中添加了更多功能,使其成为强大的安全协议:https ://www.wi-fi.org/discover-wi-fi/security

 

Q3)为什么要关注WPA3?

A3)Wi-Fi是我们日常生活不可或缺的一部分–无论是在家中,咖啡馆,办公室还是任何地方。连接安全性较弱的Wi-Fi发送数据可能会有安全隐患,因此,必须实现强大的Wi-Fi安全性,这样未经授权的用户就不能访问此数据,也不会受到诸如KRACK之类的恶意攻击。WPA3是迄今可用于Wi-Fi的最强大的安全标准。从2020年7月开始,Wi-Fi联盟将强制要求所有新的Wi-Fi认证支持WPA3。

 

Q4)WPA3安全性有哪些不同的模式?

A4)有两种模式:

1. WPA3个人:Wi-Fi个人网络用于家庭网络,Wi-Fi联盟对WPA3个人模式实施了许多安全更新,包括将SAE引入个人网络。

2. WPA3企业:WPA3企业将作为政府大楼,医院,公司办公室等中的Wi-Fi网络。它涉及在Wi-Fi®设备和接入点(AP)之间使用Radius服务器进行身份验证。

 

Q5)支持WPA3安全协议的Wi-Fi设备是否仍可以与WPA2接入点一起使用?

A5)是的,WPA3保留了与WPA2设备的互操作性。

 

Q6)哪些TI Wi-Fi设备支持WPA3?

A6)TI提供了两个Wi-Fi设备系列:

1. SimpleLink™设备为MCU RTOS系统提供Wi​​-Fi,它们具有内置的IoT安全功能,可以启用电池供电的应用。了解有关SimpleLink™Wi-Fi®设备的更多信息:https : //www.ti.com/wireless-connectivity/simplelink-solutions/wi-fi/overview/overview.html

2. WiLink™8多用途设备是支持Wi-Fi mesh,MIMO,高数据吞吐量,Linux集成了蓝牙技术的收发器。了解有关WiLink™8的更多信息:https : //www.ti.com/wireless-connectivity/simplelink-solutions/wi-fi/overview/wilink-combo-solutions.html

SimpleLink™和WiLink™8设备都将支持WPA3个人和企业版

 

Q7)TI如何在现有的Wi-Fi设备上支持WPA3?

A7)TI在无线连接领域拥有20多年的经验,不断投资更新其Wi-Fi®设备,以支持最新的安全功能。为了在WiLink™8设备上支持WPA3,TI升级了设备固件,Linux驱动程序,integrated supplicant v2.9等。对于SimpleLink™Wi-Fi设备,将大量更新集成到SDK中,更新了补丁程序等等。

 

Q8)TI Wi-Fi设备是否通过WPA3认证?

A8)TI已在内部TI实验室中对WiLink™8和SimpleLink™Wi-Fi设备进行了预认证。对于SimpleLink™设备,TI将通过提供Wi-Fi®Alliance WPA3认证来进一步向前迈进。 TI计划在2020年通过外部实验室对SimpleLink™设备进行认证。

 

Q9)我可以在TI Wi-Fi®设备上重复使用WPA3认证吗?

A9)是,SimpleLink™Wi-Fi®设备用户可以按原样重复使用WPA3认证。对于WiLink™8设备,由于它需要外部主机,因此您需要将其产品带到外部实验室进行认证。

 

Q10)我何时可以在TI设备上访问WPA3?

A10)支持WPA3的WiLink™8驱动程序发布包(版本R8.8)现在可以下载!

WiLink™8 R8.8驱动程序版本:https : //www.ti.com/tool/download/WILINK8-WIFI-NLCP

SimpleLink™Wi-Fi®设备有望在2020年第四季度获得WPA3认证

 

参考文献:

https://www.wi-fi.org/

www.wi-fi.org/.../security

www.wi-fi.org/.../protected-management-frames-enhance-wi-fi-network-security