This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100 硬件调试不通

Other Parts Discussed in Thread: CC3100

您好:

我最近设计一款无线收发装置,自己选的atmel家的cpu,wifi模块用的ti的cc3100R芯片,cc3100的电路原理图完全按照cc3100 pdf 规格书上的:Typical Application – CC3100 Wide-Voltage Mode 设计,电路原理图见附件。pcb板没有按照ti boost 板做。我现在存在的问题如下:

我公司现做一款WIFI收发器,采用了贵司的CC3100,电路图如附件所示。
并按照规格书做了PCB,
系统采用的3.3V供电,现在测得我电路板的CC3100各引脚电压是:

1、ANA DCDC IN :  Pin37=3.3V;      
     PA DCDC IN:  Pin39=3.3V;
     DIG DCDC IN:  Pin44=3.3V;     
    VIO:  PIN10=PIN54=3.3V;
2、VDD_DIG:  Pin9=
Pin43=
Pin56=1.04V;  
      VDD_PA:
   Pin33=0.202V,  Pin40=
Pin41=0.183V,   Pin42=0.212V;
      VDD_ANA:
Pin25=Pin36=Pin38=Pin48=0V;
3、40M晶振: Pin22=
Pin23=0.019V;
     32.768K晶振:
Pin51=
Pin52=0V;
4、
Pin49=0.109V
    
Pin24=0V.

我自己认为
    VDD_PA:
   Pin33=0.202V,  Pin40=
Pin41=0.183V,   Pin42=0.212V;
     VDD_ANA:
Pin25=Pin36=Pin38=
Pin48=0V;
     以上这俩组电压不对。
     还有晶振都不振。
烦你帮忙解决下问题。使CC3100正常工作。

 

cc3100 电路图.pdf