This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100使用

Other Parts Discussed in Thread: CC3100, UNIFLASH, CC3100SDK, CC3200

我现在是自己的MCU和CC3100,3100和MCU通过SPI通讯,想让3100完成无线信息的收发。

我要将这个3100设置为STA(AP)模式,有几个问题想请教下:

1.首先,通过Uniflash和烧写器,通过UART口写进3100中。

2.通过Uniflash和烧写器把getting_started_STA(AP)文件烧写进去。

这样,一上电,3100就会自动成为STA(AP)。

不知道这个理解对呢?

如果是这样的话:

1.那么这些文件都是写进那个外置FLASH里?

2.这些需要先写进去的配置文件在哪里寻找,怎么修改?

3.怎么设置就可以让这个STA接入我的AP,并且通过这个AP和另一个STA通讯?

4.固件需要升级么?

5.网上资料里面还有一个getting_started_STA5.0.2这个和getting_started_STA有什么区别?

第一次接触  很多问题都不知道  麻烦各位技术人员和大神了