This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2530 + CC2591 开启PA不成功的问题

Other Parts Discussed in Thread: CC2591, CC2530, Z-STACK

项目采用CC2530与CC2591。

协议栈分别采用ZStack-CC2530-2.5.1a与Z-Stack Mesh 1.0.0都编译过,并根据资料文件SWRA308A与SWRA290开启了PA。

硬件连接采用资料上的接口,P1.1对应PA_EN;P1.4对应EN;P0.7对应HGM。

协调器与路由编译后的现象为:P1.4》EN在发送的时候,有控制,平常为1,发送时为0;P1.1>PA_EN无动作,一直保持0状态。

终端编译后的现象:P1.4与P1.1一直保持为0状态,发送时无反应。

反复确认了#define HAL_PA_LNA 与 OBSSEL1 = OBSSEL_OBS_CTRL0 和 OBSSEL4 = OBSSEL_OBS_CTRL1;

LED的驱动,我改到了P1_0,P1_2与P1_3。

请问可能是哪里出了问题,造成PA开启不成功。