1.cc2630正常运行(即不进入低功耗时),电流一般多大? 我测出来有13mA。
2.cc2630是一上电,Radio就进入RX模式吗?,是不是意味一上电不进行任何操作,电流就有6mA?
3.cc2630手册上说接收电流6mA,发射电流9mA,是指整个芯片吗?
4.内部DC-DC和内部LDO供电模式,工作电流差异有多大?
5.有测cc2630各模式电流的完整报告吗?
望各位TI工程师指教!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1,CC2630刚开始上电的时候,应该是处于你一直搜网的状态,不停发送的电流应该在9mA多点,你板子其他部分是否也有功耗在消耗的。
2,一上电应该是不停发送beacon request,发完以后进去rx状态,接收beacon。
3,芯片以及最小系统
4,相差不大,但是应DC-DC的话,功耗会更低。
5,你可以参考CC2640的功耗测试,在硬件上和CC2630的表现是一样的,只不过运行的协议不一样。
http://www.ti.com/lit/an/swra478a/swra478a.pdf