cc2538的aes如何配置,使用的协议栈是mesh1.0.0
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VV,
您好,我再描述一下我的问题:
1、我在工程f8wConfig.cfg中使能了DSECURE=1;然后分别修改了协调器和终端的KEY(二者的KEY相同),此时协调器和终端是可以正常通信的;
2、我在工程f8wConfig.cfg中使能了DSECURE=1;然后分别修改了协调器和终端的KEY(二者的KEY不同),此时协调器和终端是可以正常通信的;
3、在工程f8wConfig.cfg中使能了DSECURE=1,并且协调器和终端的KEY相同,然后在协调器和终端中将uint8 zgPreConfigKeys = TRUE;此时协调器和终端不能正常通信了;
明白了1和2的通信是正确的,但是我感觉3也应该可以正常通信才对,不知道哪里操作错了,我是用的是CC2538的芯片,协议栈使用的Z-Stack Mesh 1.0.0
谢谢!