Other Parts Discussed in Thread: CC2591, CC2590
大神们好,小弟问一下在带PA和不带PA的情况下如何调整2530的发射和接收功率啊,最近产品在距离上出了点问题,急求啊!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
发射功率:
/* Proprietary */
#if defined (HAL_PA_LNA)
19, /* phyTransmitPower for CC2591 */
#elif defined (HAL_PA_LNA_CC2590)
11, /* phyTransmitPower for CC2590 */
#else
0, /* phyTransmitPower without frontend */
#endif
也可以通过macRadioSetTxPower函数来修改发射功率。
接收:
/* minimum receiver sensitivity in dBm (see 6.5.3.3) */
#define MAC_SPEC_MIN_RECEIVER_SENSITIVITY -85
以及
/* Threshold above receiver sensitivity for minimum energy detect in dBm (see 6.9.7) */
#define MAC_SPEC_ED_MIN_DBM_ABOVE_RECEIVER_SENSITIVITY 10