将已进行2次充放电学习的SENC文件复制到另外两个电池上,立即将这两个电池在半满状态下开始充电,充电结束后Relative State of Charge一个显示97%和99%,Tape current设置为500mA,充电器实际截止电流300mA,如何能让电池充满后Relative State of Charge显示100%? 是否需要将这两个电池包电量放尽后再充满才能更新为100%? 盼复,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
将已进行2次充放电学习的SENC文件复制到另外两个电池上,立即将这两个电池在半满状态下开始充电,充电结束后Relative State of Charge一个显示97%和99%,Tape current设置为500mA,充电器实际截止电流300mA,如何能让电池充满后Relative State of Charge显示100%? 是否需要将这两个电池包电量放尽后再充满才能更新为100%? 盼复,谢谢。
hi~
试产时发现部分电池充满后ROC为99%,查看电池状态TCA没有被置1,但FC和MCHG置1,TCA清除条件是95%,有什么建议?
我在充电快结束时不断刷新SBS数据,当充电电流减小到Taper current后一段时间,FC、TCA、MCHG这三个标志为红色且RC=FCC剩余电量百分比为100%说明电池已经满足充电终止条件,在达到充电终止条件后充电器可以继续充电(Opration CfgB中CHGFET设置为0),当充电器电流继续减小到120mA后充电结束,此时保持SMBUS通讯RC、剩余电量百分比不会变化,如果先撤除SMBUS通讯一段时间后再次通讯就会发现一些电池的RC减小、剩余电流百分比变为98%或99%。我推测是电池进入休眠后自动更新了SBS数据,因为SMBUS通讯撤除后电池SDA、SCK为低电平,静置时电流为0且[Sleep]位置1。请问有什么办法可以解决这个问题?