This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ20Z45 Full charge Capacity更新问题



将已进行2次充放电学习的SENC文件复制到另外两个电池上,立即将这两个电池在半满状态下开始充电,充电结束后Relative State of Charge一个显示97%和99%,Tape current设置为500mA,充电器实际截止电流300mA,如何能让电池充满后Relative State of Charge显示100%? 是否需要将这两个电池包电量放尽后再充满才能更新为100%? 盼复,谢谢。