做了一个转接板用于烧录Flash。Master是FT2232,IO电平固定为3.3V,Slave是一个FPGA外挂的Flash,IO电平是1.8V。所以需要一个电平转换芯片。
采用的是TXS0108E,8通道双向电平转换,用的是datasheet里面的典型电路,VCCA=1.8V,VCCB=3.3V,两边无上拉。
结果发现SPI识别不到设备,不知道是否是TXS0108E速度太低导致,上位机软件上看不到SPI的速度,无法设置。
请教大神该怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做了一个转接板用于烧录Flash。Master是FT2232,IO电平固定为3.3V,Slave是一个FPGA外挂的Flash,IO电平是1.8V。所以需要一个电平转换芯片。
采用的是TXS0108E,8通道双向电平转换,用的是datasheet里面的典型电路,VCCA=1.8V,VCCB=3.3V,两边无上拉。
结果发现SPI识别不到设备,不知道是否是TXS0108E速度太低导致,上位机软件上看不到SPI的速度,无法设置。
请教大神该怎么办?
转换的是SPI 信号吗?TXS0108能够支持的最大data rate为110Mbps,所以要看下您的SPI信号速率多大,是否TXS0108能够支持呢。
不知您的信号速率是多大的? 如果还是需要不带方向控制位的电平转换器件,可以看下LSF0108.
带方向控制位的话,速率能支持的高一点的,可以参考SN74AVC8T245。
你好,我现在也出现识别不到FLASH情况,后来你是怎么解决的,谢谢啊!