Other Parts Discussed in Thread: TXS0108E, LSF0108, SN74AVC8T245
做了一个转接板用于烧录Flash。Master是FT2232,IO电平固定为3.3V,Slave是一个FPGA外挂的Flash,IO电平是1.8V。所以需要一个电平转换芯片。
采用的是TXS0108E,8通道双向电平转换,用的是datasheet里面的典型电路,VCCA=1.8V,VCCB=3.3V,两边无上拉。
结果发现SPI识别不到设备,不知道是否是TXS0108E速度太低导致,上位机软件上看不到SPI的速度,无法设置。
请教大神该怎么办?