This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC2G86支持最高输入频率多少?

Other Parts Discussed in Thread: SN74AUC2G86

比如我想对两个350MHz的信号做异或运算,SN74AUC2G86能否完成这么高速率的运算呢?

  • SN74AUC2G86是不能实现这么高速率的运算的

  • 那么最高能支持多高速率?手册里并没有提到这一项。 我想知道限制一个门电路的工作频率的主要参数是什么? 是输出上升沿/下降沿时间和传输延时这两个参数么? 如果是的话 是怎么个换算关系?

     

  • 速率和传输延迟(tpd)这个参数有关,tpd的含义是平均传输延迟时间,这个值越小,速率越高。在有些手册中,可能没有这个具体值,可以通过这个公式计算得来:tpd=(tPHL+tPLH)/2;有tpd的值的话,我们可以根据tpd的倒数来估算一个最坏的情况,比如 SN74AUC2G86datasheet中我们看到当Vcc取不同的值时,tpd的值也不同,当Vcc=1.8V时,tpd(max)=1.7ns,那么估算下1/1.7=588Mbps(294MHz),再比如当Vcc=0.8V时,tpd=5.8ns,1/5.8=172Mbps。

x 出现错误。请重试或与管理员联系。