我想使用TPS61081芯片输出10v/180mA给LCD背光电源使用,看芯片手册上的应用电路是输出10.5V/200mA,不知道这个数字怎么计算出来的,电路中的R1,R2,Reset阻值是如何取的?SS端输入的PWM占空比与输出电流有什么关系,有具体的计算公式吗?或者是正先关还是负相关?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想使用TPS61081芯片输出10v/180mA给LCD背光电源使用,看芯片手册上的应用电路是输出10.5V/200mA,不知道这个数字怎么计算出来的,电路中的R1,R2,Reset阻值是如何取的?SS端输入的PWM占空比与输出电流有什么关系,有具体的计算公式吗?或者是正先关还是负相关?
Hi
这个电路中将参考电压通过软启动脚调整到200mV, 灯电流时200mA, 所以Rset = 200mV/200mA=1ohm.
SS电压是SS电流乘以SS电阻, 电流是5uA, 电阻是2个80kohm并联得到40kohm, 两者撑起来就是200mV。
你可以依据这个思路来设计。