This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61081用于输出LCD背光电源如何配置电路中的阻值



我想使用TPS61081芯片输出10v/180mA给LCD背光电源使用,看芯片手册上的应用电路是输出10.5V/200mA,不知道这个数字怎么计算出来的,电路中的R1,R2,Reset阻值是如何取的?SS端输入的PWM占空比与输出电流有什么关系,有具体的计算公式吗?或者是正先关还是负相关?

  • Hi  

        这个电路中将参考电压通过软启动脚调整到200mV,    灯电流时200mA,   所以Rset = 200mV/200mA=1ohm.

        SS电压是SS电流乘以SS电阻, 电流是5uA,  电阻是2个80kohm并联得到40kohm,   两者撑起来就是200mV。

        你可以依据这个思路来设计。

  • 您好,下面这个是AM437X_gp_evm板子上的背光电路,那按照这么计算背光电流,5uA * (10 || 71.5K) / 2 =0.05uA , 背光电流就只有0.05uA了,这个太小了吧,应该不合理了。如果是5uA*71.5K /2 =178mA,这个合理,但是这种计算方式又不适用于上面典型电路了,很矛盾,不知道如何计算。除此之外,那输入端的pwm占空比如何配置呢?我不知道这个PWM的频率和占空比如何确定,您能指导一下吗?谢谢。