Hi 各位大佬:
我有 TDA2Px 开发板,TF 卡 32G。我电脑是ubuntu16.04的系统,我下载了 PROCESSOR_SDK_VISION_03_08_00_00_setuplinux.bin SDK。并在ubuntu上安装成功了。
我该怎么构建编译环境,然后怎么把拷贝编译后的,以及拷贝哪些东西到 TF 卡里。
编译环境按如下方式搭建有问题么:
1) Download & install the vision SDK 3.8 . done!
2) Install package required for the build (chapter 2.2.3 Other mandatory software packages for build). done!
3) Do the below changes in the vision_sdk/build/Rules.make
MAKECONFIG?=tda2px_evm_linux_all
4) Follow the instruction provided in the user-guide for GIT configuration set-up (chapter 2.4.1 One time PC set up).
5) cd vision_sdk/build/
6) Run the below script from the build directory, this will clone kernel, u-boot, etc.
./hlos/scripts/linux/setup_linux.sh.
This refers to 2.4.2.1, do I need to go through 2.4.2.1.1~2.4.2.1.3
7)Follow the instruction provided in the user-guide for target file system set-up(chapter 2.4.2.1.4 Download and untar file system)
8)Follow the instruction provided in the user-guide for A15 compiler set-up (chapter 2.2.1 A15 Compiler, Linker)
9) make linux
10) make linux_install
11) make -s -j depend
12) make -s -j
编译生成后的文件要拷贝哪些文件并拷贝到TF的什么目录下。