Other Parts Discussed in Thread: LM5101B, UCC27211
我用两片LM5101B去驱动H桥MOS管,做一个D类功放,加上方波信号(150K方波,已经加了500ns死区延时),空载总电流300多毫安,驱动芯片发热严重,一会就烧掉了,换了一片芯片后,我先把方波信号频率降到10k没有问题,输出正常,但是频率增加到30看时驱动芯片又开始发热,后来加到100k时,一会又烧掉了,到底是怎么回事啊?求教!附件是功率级电路图。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照您的设计,看起来是LM5101B驱动能力不够,Vdd的电流等于MOS的Qg乘以频率:Id=Qg*f=50nC*100K=5mA(如果驱动输出10V左右或者说MOS, Vgs电压在10V左右,对应Qg=50nC左右,频率取100kHz), 按照LM5101B datasheet ,操作电流在3.5mA以内。
所以当频率较高时,操作电流会比较高,而且会同时驱动2个mos, 电流翻倍,超出芯片的驱动能力,同时会引起芯片发热、。
这下惨了,几片芯片都烧了,你说的那个操作电流我不是很明白,是不是指的Idd的平均电流啊?但是datasheet上说的操作电流是在500k时测得数据啊,我这只有100k就烧了,烧了的芯片Ho和HS直通了,更纠结的是开始的时候整个板子正常工作了一段时间。
之前我用的IR2110做驱动,也是总烧驱动芯片,至今也没搞明白怎么回事!
操作电流就是Idd的平均电流。驱动芯片包括电源芯片自带的驱动都是要注意驱动能力的,您选用的MOS Qg比较大,所以会造成较大的Idd电流需求。 datasheet 并没有清楚描述500kHz时的测试参数。
推荐您采用UCC27211之类的驱动芯片: www.ti.com.cn/.../getliterature.tsp
UCC27211驱动能力相对比较大,或者您需要注意MOS的选取,可以选择Qg相对较小一点的MOS.