Other Parts Discussed in Thread: LM5175, LM5175EVM
LM5175,设计参数如下:VIN 6-36V,Vout 12V,Iout(max)=6A;
当输入降到6V时,不加负载,输出稳定,加载到3A左右,输出开始震荡或掉电至5V左右;
请专家解答下,是否有办法调?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
将电路图传上来看一下。
注意输入电容建议大于100uF,并且采用多个并联,走线较宽靠近MOS输入端,毕竟此时电流有8A左右。
电感的保和电流也建议预留大一点。
感谢及时回复,原理图见附件;
输入电容是大于100uf的,电感饱和电流17A;另外,我手上有LM5175EVM的demo板,测试也存在这个情况;
备注:我测试时,R315已改为100K, C227我调大到330pf试过,无改善。