U-Boot 2010.06 (Oct 24 2015 - 03:23:43)
TI8148-GP rev 3.0
ARM clk: 600MHz
DDR clk: 400MHz
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
2048 MiB
Using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x80000, size 0x80000
524288 bytes read: OK
## Starting application at 0x81000000 ...