This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 启动到## Starting application at 0x81000000 ...就停止了,并且Hit any key to stop autoboot: 0直接跳过



U-Boot 2010.06 (Oct 24 2015 - 03:23:43)

TI8148-GP rev 3.0

ARM clk: 600MHz
DDR clk: 400MHz

DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
2048 MiB
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0

NAND read: device 0 offset 0x80000, size 0x80000
524288 bytes read: OK
## Starting application at 0x81000000 ...

  • 你好,

    能否修改uboot min的CONFIG_BOOTDELAY为3?不知道你用的是哪个软件,IPNC RDK里面请修改文件u-boot\include\configs\ti8148_ipnc.h.

    #ifdef CONFIG_TI814X_MIN_CONFIG
    ...
    # define CONFIG_SYS_PROMPT        "TI-MIN#"
    /* set to negative value for no autoboot */
    # define CONFIG_BOOTDELAY        0   --》修改为3