This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
以TMS320F28335芯片为例
在内部RAM中程序能够,达到150MHZ,也即150MIPS.
用下面这段程序测试:
for(;;) |
{ |
GpioDataRegs.GPACLEAR.bit.GPIO0=1; |
DSP28x_usDelay(29992);//29992*5+9个时钟周期 |总共300001个时钟周期
GpioDataRegs.GPASET.bit.GPIO0=1; |
DSP28x_usDelay(30000);//30000*5+9个时钟周期 |
} |
在RAM中运行上面的程序能够正常,GPIO 的周期为500HZ
在外部RAM中最大能达到多少的速度呢?
试一下,在28335中,XCLK=SYSCLK的时候。设置
XintfRegs.XTIMING7.bit.XRDLEAD = 1;
XintfRegs.XTIMING7.bit.XRDACTIVE =2;
XintfRegs.XTIMING7.bit.XRDTRAIL = 1; 也就是说XINTF读取一个外部RAM中的数据要1+3+1个时钟周期,为5
跑上面谈到的程序,GPIO的周期为100HZ,比在RAM中慢了5倍,因为RAM中读取一个数据只要1个时钟周期,外部RAM中读取要5个
改变一下:
XintfRegs.XTIMING7.bit.XRDLEAD = 1;
XintfRegs.XTIMING7.bit.XRDACTIVE = 1;
XintfRegs.XTIMING7.bit.XRDTRAIL = 0; 也就是说XINTF读取一个外部RAM中的数据要1+2+0个时钟周期,为3
跑上面谈到的程序,GPIO的周期为166.7HZ,899984时钟周期,因为RAM中读取一个数据只要1个时钟周期,外部RAM中读取要3个
理论上在外部RAM中运行最快可以为75MHZ,但一般我们只能达到50MHZ,因为一般我们不能设置.XRDACTIVE 为0
在FLASH中运行上面的程序,打开flash pipeline。会发现运行的比外部RAM还慢,只有138.888HZ的GPIO周期。
FLASH中运行程序,需要说到FLASH pipeline。
FLASH pipeline可以一次读取FLASH中的64bits,也就是正常的4条指令。那么理论上有FLASH pipeline的时候,FLASH的运行最优的速度为37 ns的FLASH介入时间乘以4,也就是108 MHz 。
但是,如果如我上面的测试代码那样充满了跳转指令(也即FLASH pipeline一次取4个指令指令后发现是跳转指令无法连续运行后面的指令)那么最坏的结果,是FLASH运行在108/4,27MHZ下。
所以,只能这样说,程序在FLASH中的运行速度为27~108MHZ,一般情况下,程序优化的还不错跳转指令比较少,在FLASH中28335的运行速度为80~90MHZ。