从开发板的SDK中复制相关的文件到自己创建的项目文件中,方便学习和使用。从点亮一个LED灯开始。
一、创建项目文件
1.1、官网获取SDK:SDK
1.2、将SDK文件中的下面文件复制到我创建的项目文件中
1.3、下面是我创建的项目文件夹
1.4、下面是创建的工程项目。
编译工程没有错误。
二、LED部分代码
2.1、LED硬件电路
2.2、GPIO驱动LED部分的代码
#include <stdio.h> // Driverlib includes #include "hw_types.h" #include "hw_ints.h" #include "hw_memmap.h" #include "hw_common_reg.h" #include "interrupt.h" #include "hw_apps_rcm.h" #include "prcm.h" #include "rom.h" #include "rom_map.h" #include "prcm.h" #include "gpio.h" #include "utils.h" // Common interface includes #include "gpio_if.h" #include "pinmux.h" #define APPLICATION_VERSION "1.4.0" //***************************************************************************** // GLOBAL VARIABLES -- Start //***************************************************************************** #if defined(ccs) extern void (* const g_pfnVectors[])(void); #endif #if defined(ewarm) extern uVectorEntry __vector_table; #endif //***************************************************************************** // GLOBAL VARIABLES -- End //***************************************************************************** //***************************************************************************** // LOCAL FUNCTION PROTOTYPES //***************************************************************************** void LEDBlinkyRoutine(); static void BoardInit(void); //***************************************************************************** // LOCAL FUNCTION DEFINITIONS //***************************************************************************** //***************************************************************************** // //! Configures the pins as GPIOs and peroidically toggles the lines //! //! \param None //! //! This function //! 1. Configures 3 lines connected to LEDs as GPIO //! 2. Sets up the GPIO pins as output //! 3. Periodically toggles each LED one by one by toggling the GPIO line //! //! \return None // //***************************************************************************** void LEDBlinkyRoutine() { // // Toggle the lines initially to turn off the LEDs. // The values driven are as required by the LEDs on the LP. // GPIO_IF_LedOff(MCU_ALL_LED_IND); while(1) { // // Alternately toggle hi-low each of the GPIOs // to switch the corresponding LED on/off. // MAP_UtilsDelay(8000000); GPIO_IF_LedOn(MCU_RED_LED_GPIO); MAP_UtilsDelay(8000000); GPIO_IF_LedOff(MCU_RED_LED_GPIO); MAP_UtilsDelay(8000000); GPIO_IF_LedOn(MCU_ORANGE_LED_GPIO); MAP_UtilsDelay(8000000); GPIO_IF_LedOff(MCU_ORANGE_LED_GPIO); MAP_UtilsDelay(8000000); GPIO_IF_LedOn(MCU_GREEN_LED_GPIO); MAP_UtilsDelay(8000000); GPIO_IF_LedOff(MCU_GREEN_LED_GPIO); } } //***************************************************************************** // //! Board Initialization & Configuration //! //! \param None //! //! \return None // //***************************************************************************** static void BoardInit(void) { /* In case of TI-RTOS vector table is initialize by OS itself */ #ifndef USE_TIRTOS // // Set vector table base // #if defined(ccs) MAP_IntVTableBaseSet((unsigned long)&g_pfnVectors[0]); #endif #if defined(ewarm) MAP_IntVTableBaseSet((unsigned long)&__vector_table); #endif #endif // // Enable Processor // MAP_IntMasterEnable(); MAP_IntEnable(FAULT_SYSTICK); PRCMCC3200MCUInit(); } //**************************************************************************** // //! Main function //! //! \param none //! //! This function //! 1. Invokes the LEDBlinkyTask //! //! \return None. // //**************************************************************************** int main() { // // Initialize Board configurations // BoardInit(); // // Power on the corresponding GPIO port B for 9,10,11. // Set up the GPIO lines to mode 0 (GPIO) // PinMuxConfig(); GPIO_IF_LedConfigure(LED1|LED2|LED3); GPIO_IF_LedOff(MCU_ALL_LED_IND); // // Start the LEDBlinkyRoutine // LEDBlinkyRoutine(); return 0; }
三、仿真程序
五、执行结果
D5,D6,D7 红、绿、蓝LED灯交替点亮,创建的项目完成,程序可以运行。