Part Number: ISO224
在使用ISO224BDWVR进行评估测试时,发现芯片输入较低电压时,增益的精度开始下降,离手册里描述的1/3的固定增益偏差较大,具体为输入1V时,输出电压0.4V,增益为0.4,误差已经很大了
在低电压区无法正常使用,请问是什么问题?手册里0.3%的精度,具体指的是哪一个,是1/3*(1±0.3%)吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.