Other Parts Discussed in Thread: XTR105
Vcm规格书上写介于1.25-3.5V之间,又写了Vcm是相对于Pin6而言的,但是我还是不理解,Vcm是那个点与Pin6之间的压差?
请高手解释下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XTR105
Vcm规格书上写介于1.25-3.5V之间,又写了Vcm是相对于Pin6而言的,但是我还是不理解,Vcm是那个点与Pin6之间的压差?
请高手解释下,谢谢
你好!
首先可以明确的是Vcm是表示共模电压,在datasheet的规格书中1.25-3.5V表示共模电压的范围,在我们一般的电源中,一般都是有电源,有参考地,故我们的电路中的所有的电压值都是参考地来计量的,而在此处的,我们的Vcm就是参考PIN6来计量的。而Vcm不是表示哪个点与PIN6之间的压差,此处的Vcm同样表示共模电压范围,只是其参考点是PIN6。
谢谢!
下图是XTR105的典型应用中的输入部分。

RTD上的驱动电流的Rz上的驱动电流通过电阻Rcm流入到Iret.XTR105的输入端可视为一个仪表放大器。它通过测量由RTD阻值变化而引起的电压变化,这个电压是一个差模信号。
差模电压直接输入到仪表放大器的输入端。同时这个差模电压上有一个共模电压,加在Vin-上。它是由2IR流过Rcm形成电压和IR流过Rz形成的电压之和。所以它是相对于PIN引脚Iret测量的。这个共模电压会对器件的输出电流有所影响。datasheet上给出了这个共模电压在1.25-3.5V范围内,它的变化对器件输入输出参数的影响。从数据中可以看出,它的影响是非常小的。