Other Parts Discussed in Thread: ISO124
请教:隔离放大器ISO124用+-5V供电,最高线性输出电压能到多少?手册只有在+-15V时的。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO124
请教:隔离放大器ISO124用+-5V供电,最高线性输出电压能到多少?手册只有在+-15V时的。谢谢!
非常小,可以简单认为不管是5V供电还是15V供电,输出幅度比电源电压低的程度是一样的,也就是说差不多典型值2.5V,最小值很小。
谢谢上面各位答疑!
我的应用是:ISO124后接有源滤波再进入3.3V供电AD(MCU自带)。
也就是说为保证最高3.3V信号电压,ISO124供电应有3.3+4.5,在7.8V以上?
再次请教:
mV信号经通用运放构成的仪表放大器放大,由ISO124隔离,再通过运放有源滤波送入AD.
请教,这隔离的两部分电路,分别直接用隔离型DC/DC电源模块供电,是否合理,满足纹波等技术指标?
谢谢!