Part Number: OPA735
需要设计一款电刺激模块,用32单片机的DAC控制电流输出范围为0-10MA可调,负载外接(活体负载),负载阻抗可以达到几兆欧,请大佬提供思路,谢谢。目前参考OPA735电路的设计,但是接入负载后没有电击效果。
OPA735电压调节电流电路.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA735
需要设计一款电刺激模块,用32单片机的DAC控制电流输出范围为0-10MA可调,负载外接(活体负载),负载阻抗可以达到几兆欧,请大佬提供思路,谢谢。目前参考OPA735电路的设计,但是接入负载后没有电击效果。
OPA735电压调节电流电路.pdf
谢谢您的回答,我想通过这个电路实现电刺激,类似于将两个电极接到让人体手臂,用微小电流进行刺激(0-10ma可调),现在我这边是电流可以调节,接上负载后就没有电流流过了,达不到刺激效果。
谢谢您的回答,我想通过这个电路实现电刺激,类似于将两个电极接到人体手臂(一个电极对应一条手臂),用微小电流进行刺激(0-10ma可调),现在我这边是电流可以调节,接上负载后就没有电流流过了,达不到刺激效果。
谢谢您的回答,我想通过这个电路实现电刺激,类似于将两个电极接到让人体手臂(一个电极对应一条手臂),用微小电流进行刺激(0-10ma可调),现在我这边是电流可以调节,接上负载后就没有电流流过了,达不到刺激效果。
这是医疗级的申请。对于肌肉刺激应用,根据皮肤状况,施加在人体皮肤上的最大安全电压约为60Vdc范围,在脉冲直流、双相脉冲(AC)应用中,用于刺激的最大安全电流小于10mA。我不记得TI的应用说明中讨论过肌肉或神经刺激的应用。我知道许多以前的传感应用都是基于EEG/EKG/EMG相关的电压传感测量。
我认为以下申请说明不适合医疗申请。
对于肌肉/神经医疗刺激应用,变压器通常用于将电有源电路与人体隔离,再次保护触电、接地回路和设备故障。这是对交流/脉冲供电的人机接口电路的具体要求。
我没有做任何与此特定应用程序相关的设计或支持,我需要调查一下。请根据您的刺激应用程序确认上述描述是正确的。
我在E2E上发现了一些双相关系应用查询。