Other Parts Discussed in Thread: LMP7721
想用LMP7721做电离室的电流放大电路,使用最简单的反相放大器输入电路,±2.5V电源,线性稳压电源,保证电源的干净。现在问题是,当输入为0时,输出大概有-30mv的输出。这个需要设计调零电路吗?
另外,我想只使用1个反馈电阻,100KΩ来满足6个量级电流的放大(10E-11A----10E-5A),LMP7721能不能实现。请大神们帮忙分析一下。
附件是电路图。谢谢了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMP7721
想用LMP7721做电离室的电流放大电路,使用最简单的反相放大器输入电路,±2.5V电源,线性稳压电源,保证电源的干净。现在问题是,当输入为0时,输出大概有-30mv的输出。这个需要设计调零电路吗?
另外,我想只使用1个反馈电阻,100KΩ来满足6个量级电流的放大(10E-11A----10E-5A),LMP7721能不能实现。请大神们帮忙分析一下。
附件是电路图。谢谢了。
能否胜任不仅取决于LMP7721,还和后续电路有关,例如,后续的放大器、ADC等它们的漂移、噪声等都对测量有影响,另外一方面还看你的系统对于带宽的要求、对于测量精度的要求等等。我感觉测量5个数量级是有可能的。因为通常而言电离室信号变化很慢,接近直流,将整个系统的带宽限制在比较窄的范围还是比较容易将噪声降到1uV内的。
1mV纹波应该是足够了,即使它进入到信号里面我们还可以用数字滤波来滤除它。
我讲的系统带宽当然包括整个信号链路的带宽,即放大器和ADC,可以再MCU内软件实现的数字滤波器将带宽降低到满足需要的水平。带宽越窄噪声越低但响应速度会越慢,需要在两者之间妥协。
还是要限制一下,不然高频部分会在ADC采样时混叠到低频,数字滤波器就无能为力了。具体要限制到多高频率那就要看ADC的特性了。
LMP7721的零点偏差是+/-180uV(25°C)或+/-480uV(-40°C到125°C),超出此范围就不正常了。有很多原因会导致过大的零偏,比如PCB泄露、外界干扰、PCB应力、导线的热电偶效应等等。需首先将这些外部因素排除。芯片自身的零偏只能通过校准补偿了,用软件补偿即可。但它会随温度、时间漂移的,最好能在系统进行动态补偿。