This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM359: LM359可否应用电压跟随器,做一个缓冲极

Part Number: LM359


Subject: Inquiry Regarding Using LM359 as a Voltage Follower

Dear TI Support,

I’m considering using the LM359 op-amp in a voltage follower (unity gain buffer) configuration.

My application involves a single-supply system with V+ = 12V and V− = 0V (GND), and I need to buffer signals in the 0V to 12V range.

Could you please confirm whether the LM359 is suitable for this use case?

Specifically:

  • What are the input and output voltage ranges when operating on a single 12V supply?

  • Is it possible to achieve reliable buffering down to 0V or up to 12V without significant distortion?

If the LM359 is not ideal for this, could you recommend a suitable high-speed op-amp with rail-to-rail input and output?

If possible, it would be very helpful if you could also provide a basic simulation schematic or test circuit example for reference.

Thank you very much for your support.

Best regards,
[SUN]