This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
OPA462: OPA462
Part Number: OPA462
可以使用150V和-10V这种供电方式吗
您好
根据您的问题说明,您应该是需要单端,但是根据datasheet说明单端范围是a single supply of 12 V to 180 V
我是要双电源供电,但是VEE是负10V,VCC是150V,这种
如果您这样做会比较接近极限,建议用以下方式仿真一下
www.ti.com.cn/.../sbomav9