This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

麥克風差動訊號放大電路

Other Parts Discussed in Thread: OPA1678, RES11A

Hi experts,

能請建議適合的差動訊號方大方案嗎?  

  1. 麥克風差動訊號(來源為壓電感測器)輸出範圍:uV ~ mV  
  2. Gain 值 : 25-40 dB (因為每一顆麥克風的接收靈敏度皆不相同,因此需要可調整式的Gain值)
  3. 頻帶範圍:20 Hz ~ 256 kHz,  帶通濾波器通帶內增益變異度 ±2.5 dB 以內. 如果20Hz以下的訊號無法濾波,可以只實現256KHz以下的低通濾波器.
  4. 雜訊設計目標:等效雜訊電壓 < 100 nV/√Hz
  5. 輸出介面:Single-ended 輸出
  6. 外部可以供電電源為+12V. 電源設計如果方便也請提供建議.

Thanks,

Allan