This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4354: 放大器论坛

Part Number: OPA4354
Other Parts Discussed in Thread: OPA4325, OPA365, OPA354

Why does the OPA4325 perform better than the OPA4354 when the input is below 100 mV? My circuit is attached below. The DC input is applied at pin 10, and I'm measuring the output at pin 7. As shown by the dotted line, the OPA4325 provides better linearity. Why is that?

  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • The main difference between the OPA4354 and OPA4325 is the Voltage output swing from rail. The OPA4354 has typical value of 100mV from the rails while OPA4325 has typical of 10mV from the rail. Hence, you are seeing non-linearity for inputs <100mV for OPA4354. We are working on a new amplifier OPA4620 which swings close to output rails. The circuit is a peak detection circuit.

    1. What is the minimum peak that you want to detect?
    2. What is the required speed? 

    We also have OPA365, which is a zero cross over, 50MHz amplifier with output swing from rail <20mV across temperatures.

  • In our application we need to detect signals as small as 60 mV, with a required bandwidth of about 2 MHz. Could you clarify which datasheet parameter you are referring to in your explanation? Is it the 'Voltage Output Swing from Rails'?

    Also, why is the OPA4325 able to swing closer to the supply rails (≈10 mV) compared to the OPA4354 (≈100 mV)? What design or architectural difference enables this improvement?zero-crossover input stage?

    Could you clarify the relationship between the zero-crossover input stage and the output voltage swing from the rails? what are the key output-stage differences between OPA365/OPA4325 and OPA4354 that lead to ≈5–10 mV vs. ≈100 mV headroom?

  • I am sorry for not being clear before. Yes, I was talking about 'Voltage Output Swing from Rails'. There is no relationship between the zero-crossover input stage and output voltage swing from rails. However, the key difference between the OPA365/OPA4325 and OPA354 is that OPA354 has an extra circuitry to have one of the best overload recovery time which restricts the output swing to 100mV from supply rails.

    I would suggest OPA365 for its

    1. Output swing closer to rails that enables detection of 60mV
    2. It has sufficient bandwidth
    3. Good DC precision enabling less offset error at output.
    4. Zero cross over enabling Wider input range without cross over distortion.
    5. Low bias current for peak detectors.
  • Thanks for the reply. since OPA365 did not drop-in for OPA4354(old design) Could we use the OPA4325 instead of OPA4354?

    I am not very clear about this parameter 'Voltage Output Swing from Rails'. how to simluate this parameter? Are there key design trade offs ? that influence  why some OPA can swiing closer to rails~10mV like OPA4324 but like OPA4354 ~100mV?

  • OPA4325 is a lower bandwidth device with 5V/us slew rate. For peak detection, high slew rate and bandwidth is required. What is the fastest frequency of the input?

    As mentioned before, we are releasing OPA4620 which is drop in for OPA4354 and will be the right fit. 

  • May I know who is the customer and what are the project timelines?

  • The festest frequency is about 1.2Mhz. When will OPA4620 release? 

  • Could you advise how to simulate the difference for Voltage Output Swing from Rails in LT-spice or Tina?

  • May I know your company name and what are the project timelines?

  • Could you set this email thread as private?

  • You can share in private message