Part Number: JFE2140
Other Parts Discussed in Thread: , OPA202, OPA1637
工程师您好!
为了稳定传输信号,我需要一个具有差分输入输出的超低噪声前置放大器,请问可以在此电路上进行修改吗?如果可以,您有修改的建议吗?
期待您的回复,谢谢!2728.JFE2140_single.TSC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我编写了应用程序注释SBOA563,并创建了评估模块,该模块与JFE2140EVM的电路相同。电路的增益由以下因素控制

最大增益为1000V/V,但可以降低。我建议降低增益,将RG2保持在10欧姆并降低RF。这样,回望栅极的总电阻值更小,电阻的热噪声也更小。
为了稳定起见,电容器可以与RF并联放置。下面你可以看到我为此在EVM上放置了占位符。为了稳定起见,我还在OPA202的输出端添加了一个可选的隔离电阻器(R3)。默认配置如下所示,DNP组件是可选组件,为客户提供了足够的灵活性进行实验。

我在下面的应用笔记中的测量也使用了这个EVM。

我错过了它需要差分输出。我附上了几年前的模拟,显示了我所做的FDA配置。在这篇文章的底部找到模拟。在OPA1637电路之前,它可能应该有直流阻断帽。我还在EVM上测试了一个偏移校正电路,用于微调JFE Vgs失配。