Part Number: LM2903
Other Parts Discussed in Thread: LM339
LM2903PSR的VCC供电5V,IN-接2.5V,IN+经过30k电阻,输入一个频率为2kHz的正弦波,峰值26V,有如下问题,帮忙解答,谢谢。
1、IN+峰值26V,芯片是否会损坏?是否有影响
2、比较器的输出是否正确?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1:不会损坏。输入电压最高可达30V而不会造成损坏。但它们超出了输入电压范围。对于A1,输入范围为VCC-2V,即3V。
2:也许吧——在大多数情况下,是的,应该是正确的。见应用说明。
这依赖于LM2903系列的一个“特性”,即只要一个输入在有效范围内,输出就应该是正确的。
请参阅LM339系列应用说明的第6.4节和第6.7节:
Application Design Guidelines for LM339, LM393, TL331 Family Comparators
建议将输入电压保持在有效输入范围(0至3V)内,并且不要依赖某种“特性”,因为这种行为是不受保证的。