This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电机相电流信号采集问题

大家好,我现在使用的电流传感器是lem的LTSR 25-NP,其中电流和输出电压关系是:v=2.5+0.025*I,现在的AD采样输入范围是0-3V,中间有一个放大倍数,但是即使这样,电压稍微波动一些,计算出来的电流误差就特别大,请大家支招,谢谢!

  • 亲;这个LEM需要用一个5V的稳压电源。且量程要与你的实际相当。通常这样做后;误差会小于1%。不知你是如何选的。

    如果你觉得电源对此的影响不可接收;建议用双电源供电LEM吧。

  • 谢谢,我现在使用的5V电源的适配器供电的,供电电压在5.3V左右,并不是5V的稳压电源,这可能造成我的LTSR 25-NP输出电压不稳定的原因,而且最令我我不理解的是,我改变了它的接线方式, 但是它的输出电压的方式并没有改变,还是按照2.5+-0.625量程输出,不知道您遇到过没有