This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于PGA281疑问

大家好,麻烦大家解答一下我心中的疑问。

1、首先我采用VSP=15V,VSN=-15V。VSOP=5V,VSON=-5V。DVDD=3V供电,VOCM=0V。但是输出总是低于我实际的放大倍数。如下图:

请帮我解答一下为啥?增益控制是3V和0V。

2、我采用VSP=15V,VSN=-15V。VSOP=5V,VSON=0V。DVDD=3V供电,VOCM=2.5V。但是输出正常,如下图

请大家帮我解答一下疑惑。。我没有做阻抗匹配这些,只是仿真一下,会不会有影响。