我要放大的信号是直流,范围大概0-225mv左右,想使用仪表放大器进行放大。想选择单电源供电,这样电路可以简单一些,看了INA333,但是他的输入是(V-)+0.1V到(V+)-0.1V,如果仪表放大器的V-接地的话,有效放大的输入范围应该是从0.1V开始,这样理解对吗?如果是这样的话,那对于0-225mv的信号,应该选择什么样的仪表放大器?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对的,如果V-接GND的话,最小输入电压为0.1V。
你想放大0~225mV 信号,那么打算放大多少倍?供电电压为多少?
1. 此处所说的输入信号范围起输入形式是单端还是差分方式?
2. 信号输出阻抗特性如何?信号频率范围
3.如果考虑用INA333放大的话,需要考虑共模信号是否满足要求,简单接地可能会有问题。用双电源供电的仪表放大器可以规避以上限制
考虑到单电源运放无法处理0电位附近的信号,建议采用双电源运放。仪表运放的话,可以看下INA122。Lene 说:因为后面要接单片机的ADC,应该只要放大10倍左右。供电电压选5V。