This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3491: +12V转-12V器件选型

Part Number: THS3491
Other Parts Discussed in Thread: LM27761, LP2992, LM1117

老师们好,现在我需要使用THS3491这款芯片,打算用±12V供电,目前我只有+12V的电源,想使用逆转芯片将其转换成-12V,麻烦问一下各位老师们有什么好的建议吗
我目前的一套电源转换流程是这样的:

LT1962:12V-->5V
LM27761:5V-->-5V
LT1964:-5V-->-2.5V
LP2992:12V-->5V
LM1117:5V-->2.5V