This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP07放大器 调零有问题

Other Parts Discussed in Thread: OP07

请问一下,我使用OP07放大器,连接图如下,当传感器的输入信号为零时,使用万用表测量输出电压不为零,然后我使用1,8脚接20K欧电位器,进行调零,结果输出端的电压和之前是一样的,没有变化。不知道这是为什么(放大器可以正常工作放大,只是不能够调零)。

  • 亲;这是一颗双电源放大器,只有对称双电源供电时;输出零电压。建议要么用双电源供电;要么以2.5V为参考零电压。

  • 请问一下,以2.5V为参考零电压是否就是将放大电路中接地的地方换成接2.5V?

  • 1、当双电源供电时, 传感器输入信号为零,输出的数据为0.37V?

    2、在1的前提下,我在放大器的1,8脚之间接入20K欧的电位器调零,并没有作用

  • 确保你处供电正常(双电源)情况下,请将应用电路贴上来,并且根据以下各条做检查。

    > 输入信号的特性,输出幅值、频率范围、输出阻抗

    > 运放电路拓扑结构、输出负载

    >如何测量得到的数据?示波器还是万用表

    另外,运放1脚与8脚之间电位器用于调整失调电压,只能在小范围内变化。

  • 放大电路的输入信号:幅值:8mV,输出阻抗1000欧

    得到的数据使用万用表测量的

    另外有一个疑惑:放大器实际的放大倍数和理论放大倍数总是相差一大截,比如理论放大200倍,但实际只有130倍左右,这是正常的现象吗?