This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2901: 是否支持负压输入

Part Number: LM2901
Other Parts Discussed in Thread: TLV1872, SN74HC08, LM311, LM6511

你好,我目前使用LM2901比较器,该比较器的供电电源正为12V,电源负为-12V。输入IN+、IN-可能存在负压-2V。有如下两个问题:

1、LM2901DR是否支持正负电源供电,即SOIC-14封装的第3脚VCC接+12V,第12PIN脚GND接上-12V。

2、在如上供电的情况下,IN+与IN-是否支持负压输入,如-2V等,我目前测试中输入给负压时发现LM2901DR芯片未损坏,但老化一段时间后,发热特别大,芯片表面温度可达90℃。如果IN+与IN-给的都是正压,芯片发热正常。

  • 您好,已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 是的,LM290x系列可以使用“分体式”电源供电。但需注意输出特性。
    若V+为+12V,GND为-12V,则应能支持-12V至+10V的输入电压范围。
    输出驱动是什么?当LM2901输出为“低电平”时,其电压为-12V(输出端接地至“GND”引脚,该引脚电压为-12V)。下一级电路能否接受-12V输入?
    听起来像是输出端通过ESD二极管钳制到系统地(0V),导致输出端流过大电流。
    请提供完整的原理图,包括输入和输出电路。
    该设备在正常运行下,最坏情况下升温不应超过一两度。..
    若上述情况成立,建议参考TLV1872,该器件专为双极电源设计,具备接地参考逻辑输出功能。
    本周站点将因圣诞假期停业,因此我们的回复将推迟至下周。

  • 如图所示,LM2901的输入是一个信号经过低通滤波后与4路参考电压进行对比。输出是接到一个与门SN74HC08。

    当LM2901输出为高电平时,该电平是通过上拉电阻接到3.3V。

    当LM2901输出为低电平时,是使用一个1N4148将低电平(也就是-12V)拉到-0.4V。

  • 看起来发热是由LM2901输出端的大电流下拉引起的。当LM2901输出低电平(IN- > IN+)时,其输出端试图将输出电压拉至LM2901接地引脚(-12VA)的电压水平。然而,当输出电压低于DGND时,输出端由输出二极管(D1、D3、D5和D7)正向偏置形成二极管钳位。这很可能导致LM2901吸收大量电流并产生自发热。若测量二极管温度,相信它们同样会相当烫手。我认为发热问题并非源于LM2901输入端的负电压,而是输出低电平状态导致输出二极管正向导通,从而使LM2901承受了过大电流。

  • 好的,谢谢,如果选用支持负压输入,输出低电平为GND的比较器,比较常用的就是TLV1872吗?

  • TLV1872是现代替代品,无需上拉电阻。

    传统分压供电方案采用LM311、LM319或LM6511,其“浮动”开集输出通过接地“GND”引脚实现接地基准逻辑。

    若在分压供电中使用LM2901,则需在输出端进行电平转换。通常在拉高电阻中添加第二只电阻,形成“低电平”时的分压电路(例如使“低电平”分压点电压接近0V)。该电阻应置于输出端与二极管结之间,二极管可保留以防止输出电压过低跌破地电平。

    因此低电平总输出电压为-12V + +3.3V = 15.3V。需设计分压电路使低电平时产生0V分压点。该分压器需从15.3V中提取12V分压点。快速计算可知:若在输出端与上拉电阻/二极管结点间接入36.5kΩ电阻,则低电平时输出电压将接近0V。

  • 好的,非常感谢