Part Number: BUF802
Hi, Team:
I used BUF802 in my design, V+ was connected to PP8V5,V- was connected to PN4V5. In datasheet input range spec. is 4.5Vpp@450MHz, what is range BUF802 support? May input range set to 6Vpp?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BUF802
Hi, Team:
I used BUF802 in my design, V+ was connected to PP8V5,V- was connected to PN4V5. In datasheet input range spec. is 4.5Vpp@450MHz, what is range BUF802 support? May input range set to 6Vpp?

您好,
BUF802是单位增益缓冲器,图中是基于VS = ±6 V,在f = 500 MHz 情况下,支持输入电压典型为4.5Vpp. 当频率越高,输入电压范围越低。
根据数据手册5.7 Typical Characteristics的频率响应特性,450MHZ与500MHZ的频率响应特性差不多,很难达到6Vpp。
BUF802 Wide-Bandwidth, 2.3nV/√Hz, High-Input Impedance Buffer datasheet (Rev. D)
您好,
我有关注到datasheet里面提到4.5Vpp@450MHz
应该是是4.5Vpp@500MHz吧
我可以牺牲带宽去满足这个输入范围吗?
从电平上来说,芯片是支持的。您可以选择牺牲带宽,建议您先仿真一下。
Choosing an Amplifier for Wide Bandwidth, High-Impedance, Data Acquisition AFEs