Other Parts Discussed in Thread: OPA656
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
首先推荐一份运算放大器的单电源供电资料,其内容中的使用说明基本上涵盖了OPAXXX系列可用于单电源供电的芯片,详细的可参看附件。
对于你说的输入端提供VCC/2的偏置直流电压,可能差分输入信号的单端输入需要更多地考虑这个。平常的单端供电芯片(非rail-to-rail芯片)只需要考虑其实际的输出电压范围。
手册14页提到的是推荐+/-5V工作,在单电源工作时,某些指标和性能会和双电源工作下测试数据有出入。建议你用TINA先做一下仿真,以确定直流工作点和交流性能是否能满足你的要求。模型可以在一下网站找到。
另外你的供电方案是用12V蓄电池后接一个10V LDO,可能存在的问题是LDO的dropout电压可能有0.3V或者更高,如果是0.3V,意味着你的蓄电池电压掉1.7V到10.3V的时候,LDO输出电压就要开始下降了。同时LDO的功率管也会逐渐的进入线性区,造成PSRR降低。所以建议你先评估一下蓄电池电压可能会掉到什么程度,注意OPA656手册上提到8V单电源供电也是可行的。
对于是否选用单电源供电,我想除了应用方便外,还要考虑你的系统是否允许用单电源供电。比方说电压输出范围,单电源供电时,OPA656是低边输出是不能到达0的。从你前一个问题上看,OPA656是用于传感器的调理电路的放大器,这个有没有对电压范围的要求呢?建议你能把传感器部分需求描述清楚。
传感器的调理电路的输入是 感应电荷信号, 幅度在+-几十毫伏的量级,单电源时不能实现0输入 0输出是系统不能容忍的 ,还是应该考虑双电源方案