This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

继续追问:OPA656的单电源供电问题

Other Parts Discussed in Thread: OPA656

  • 上次提问,您提到这是一个双电源供电的芯片,不提倡使用单电源,我在细看datasheet后发现在14页 提到可以使用8-12V的单电源供电

    对于单电源供电,能否提供典型应用电路和注意事项?

    如果能使用单电源,将使得系统设计变得非常简单,在12V的蓄电池后接一个10V的LDO即可满足

    在看单电源运放的应用电路时,通常要求在输入端提供VCC/2的 偏置直流电压,不知道OPA656是否也需要?

    麻烦解答,谢谢了!

  • 你好!

    首先推荐一份运算放大器的单电源供电资料,其内容中的使用说明基本上涵盖了OPAXXX系列可用于单电源供电的芯片,详细的可参看附件。

    对于你说的输入端提供VCC/2的偏置直流电压,可能差分输入信号的单端输入需要更多地考虑这个。平常的单端供电芯片(非rail-to-rail芯片)只需要考虑其实际的输出电压范围。

    运算放大器的单电源供电.pdf
  • 手册14页提到的是推荐+/-5V工作,在单电源工作时,某些指标和性能会和双电源工作下测试数据有出入。建议你用TINA先做一下仿真,以确定直流工作点和交流性能是否能满足你的要求。模型可以在一下网站找到。

    www.ti.com.cn/.../opa656

  • 另外你的供电方案是用12V蓄电池后接一个10V LDO,可能存在的问题是LDO的dropout电压可能有0.3V或者更高,如果是0.3V,意味着你的蓄电池电压掉1.7V到10.3V的时候,LDO输出电压就要开始下降了。同时LDO的功率管也会逐渐的进入线性区,造成PSRR降低。所以建议你先评估一下蓄电池电压可能会掉到什么程度,注意OPA656手册上提到8V单电源供电也是可行的。

  • 对于是否选用单电源供电,我想除了应用方便外,还要考虑你的系统是否允许用单电源供电。比方说电压输出范围,单电源供电时,OPA656是低边输出是不能到达0的。从你前一个问题上看,OPA656是用于传感器的调理电路的放大器,这个有没有对电压范围的要求呢?建议你能把传感器部分需求描述清楚。

  •      传感器的调理电路的输入是 感应电荷信号, 幅度在+-几十毫伏的量级,单电源时不能实现0输入 0输出是系统不能容忍的 ,还是应该考虑双电源方案