Other Parts Discussed in Thread: THS4509, ADS5463
使用THS4509和ADS5463做直流耦合采样,完全参考的ADS5463手册第27页,figure51的参考电路图,运放单电源供电。现在调试发现,当输入端悬空的时候,运放的输入端P和N的偏置电压都是2.4V(和ADS5463的VREF一致)。当接到信号源时(输出阻抗50欧),ADC采数不对,运放的PN输出有削波。运放的输入PN,偏置被信号源拉低了。
当在信号源和运放之间加隔直电容后,运放输出正常,偏置电压正常,运放的输入PN和输出PN偏置电压都是2.4V。
或者信号源和运放不隔直,信号源输出信号设置偏置电压1.2V,运放和AD都可以正常工作。
为什么按照figure51的电路测试就有问题?数据手册给的电路图不是直流耦合方式吗?有别的特殊要求吗?
请专家能解答一下,多谢。