Part Number: TLV3401
Other Parts Discussed in Thread: TLV3701
Hi 评估使用TLV3401IDBVR作为一个电压比较,输出口上拉电阻规格书推荐是1M,芯片的供电目前是8~13V之间,想问下当输出为高时候,这个时候的输出电流能力如何?有看到输出低的图例说明,输出高只是看到Rating最大10mA。输出口是开漏,例如8V供电,输出上拉电阻1M,那么给后极的供电能力是不是可以理解为8V/1M=8uA?
目前要求芯片供电8~13V之间,输出高的电流1mA左右,输出低电压小于0.5V,看下是否有合适的比较器推荐?