电路图如上图所示,这是一个电荷放大电路,电阻部分我采用了T型结构来替换需要的大电阻,其中C2是我的电容传感器,为了提高测量精度,现要对其进行噪声分析,但一般的噪声分析都是纯电阻电路,现在我的电路中有电容,需要考虑进去吗?我的信号范围是100~3500Hz。还有一个问题是计算噪声电压时候还得考虑噪声带宽,那么这个带宽是指我的运放的单位增益乘以1.57还是经过后级低通滤波之后的带宽?因为我最近想把原来的OPA347换成OPA344,可是OPA344的带宽有1MHz,OPA347只有350KHz,那么带宽越大噪声会有更多的噪声引入吧,有点矛盾。所以请教大家一下,谢谢。