This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
第二个图的问题应该和第一个一样的,建议改一下(Time/Div)应该就对了。
至于你说的10M里面有些杂波,能否直接上传波形图,这个可能是50HZ的工频干扰之类的,可能要看你的实际波形图及测试参数来判断。
自激波形的频率与输入频率应该是没有直接关系的,自激的产生是要满足以下条件:AF=-1,即|AF|= 1和arg(AF)=φA+φF=±(2n+1)π(n=0,1,2,…)。
检查电路是否稳定工作的方法:
(1) 方法一:根据AF的幅频和相频波特图来判断。设LAF=20lg|AF|(dB)
1) 当 Δφ=-180°时(满足相位条件):若LAF<0,则电路稳定;若LAF≥0 (满足幅度条件),则自激。
2) 当|AF|=1,即LAF=0dB时(满足幅度条件):若|Δφ|<180,移相不足,不能自激;若|Δφ|≥180°,满足相位条件,能自激。
3)LAF=0时的频率为f0,Δφ=180°时的频率为fc,当f0 用上述三个判据中任何一个判断均可,需要注意的是,当反馈网络为纯电阻时,反馈系数F为实数,AF的波特图与A的波特图成为相似形。为简便起见,通常只画出A的波特图进行研究。因为F为已知(或可求),20lg(1/F)是一条水平线,它与A的幅频波特图相交于一点,这交点满足|A|=1/F,即|AF|=1(对应于20lg|AF|=0),根据交点处的相位小于-180°就能判断稳定与否。
(2)方法二:只根据幅频特性,无需相频特性的判别法。
因为20lg|AF|=0时,Δφ=-180°产生自激。幅度条件改写成:20lg|A|+20lg|F| =0即:20lg|A|-20lg1/|F|=0,20lg|A|= 20lg1/|AF|≈20lg|Af|。因此,自激条件又可描述为,当Δφ=-180°时,如果开环增益近似等于闭环增益将自激。而开环增益的-20dB/dec段,对应于Δφ=-45°~- 135,-40dB/dec段对应于Δφ=-135°~- 225°。所以在开环幅频特性的波特图上,直接画闭环增益曲线,并令两者相交,若交于 -20dB/dec段对电路稳定,交于-40dB/dec 段时,电路可能自激。
如果你使用跟随器,输入是10MHz,输出也是10MHz,这样的肯定不是自激振荡。
测量有很多杂波,这个原因有很多,例如你的电源不是稳压电源,可能会出现50HZ干扰或者较强的电源纹波等。一般需要对杂波进行测量,才能找到干扰源。
10MHZ,只要你的示波器能测量,探头一般还好,不过你校正一下探头也是可以的。