This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL064单电源供电的问题

Other Parts Discussed in Thread: TL064

你好!我们的一块板子上,运放使用的是TL064,单电源+5V供电,板子对动态范围的要求不高,运放输出信号幅度不会超过2.5V,请问使用低压单电源供电,还会有其他的负面影响吗?

  • 运放单电源供电时,主要是考虑需要把信号抬升起来提供一个偏置,另外就是考虑运放的输入输出电压范围。

    TL064在+-15V电源供电时,电输入电压范围是-12V到+15V.输出电压范围+-13.5V,这就说明在输入和输出极有距离电源轨有3V的范围。当使用+5V供电时,输入端的电压范围推测为不会大于太大(3V-5V)。输出电压范围为1.5V-3.5V。还是推荐提高供电电压范围。或者推荐使用OPA3XX系列的单电源轨到轨运放。

  • 1. 手册第5页提到供电范围是+/-18V,故单电源5V供电应该问题不大。

    2. 手册第4页提到这个运放是P管输入,所以输入端的直流偏置建议给在稍小于2.5V的位置。

    3. 输出端应该没问题,毕竟你的输出摆幅只有不到2.5V。