Other Parts Discussed in Thread: LMH5401
需要测量两路1HZ-100MHZ,22mVpp-1Vpp的频率(输入为方波和正弦波),以及这两路信号的相位差,以及10MHZ的方波的占空比,占空比精度要求10%
因为信号频率最低1HZ,因此不能用交流耦合,本来是前面稍微放大了一下,后面直接接1GHZ带宽的迟滞比较器,但是中频特性很差(30MHZ衰减比较大),现在想着是不是可以直接用一片LMH5401开环放大后进FPGA的差分IO口,但是现在有两个问题:
1. 输入信号交流信号,需要在上面叠加一个1.67V的直流分量并且3.3V限幅后进FPGA,限幅的话把LMH5401的供电电压设置为+3.3V和-1.7V,然后Vcom设置为1.67V(通过3.3V电阻分压得到),仿真得到的输出电压范围149mV-3.14V,仿真看来是可行的。但是在输入信号有噪声的情况下会不会出现信号在0电平附近变化时输出信号会上下摆动?
2. 怎样得到-1.7V-3.3V电源比较经济?