Other Parts Discussed in Thread: LM4890, LM6152, OPA551
您好,我想实现这样一个功能:DA输出的模拟电压范围为0到5V,但由于此模拟IO的的驱动能力很差,最大只有4mA。所以我想在DA转换后加一个功率放大器,实现电流放大功能(输出电流最大只需要30mA就行)。要求所提供的功放最好能实现24V供电(我想让0~5V 输入时输出为0~24V,能达到20V左右都行),外围电路简单。举个例子吧,类似于LM4890这样的功能,但是它的供电电压范围最大才6V。我想需要一个供电电压能达到24V的。
谢谢啦!请TI工程师给点建议吧~