This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

锁定放大器相敏检测部分出现不可思议的现象,求大家帮忙解释下 ,感激不尽!

Other Parts Discussed in Thread: LM358

锁定放大器4053部分如图所示 给电路板只上+-5V的时候 4053逻辑是正确的 4和15脚输出波形互补(正常)但一旦例外供上+-12之后 就会出现逻辑功能错误的现象,4和15波形一样了(不正常)  图中的LM358AD我用的是LM358,例外 当吧358的5,6脚与4053的4和15断开之后发现功能又正常了 ,但是4053的4脚的峰峰值只有0.8V(Vo为1KHZ Vpp为1.8V,控制信号为+-5V频率为1khz的方波) 15脚为1.8V 频率都为1KHZ。之前电路板做出来的时候是好的(上+-5V和+-12之后) 但如今测就出现了问题。。求各位路过的亲朋友好友帮忙解答 谢谢各位了 在线等 急急急!